Unwrap Reference (Trace Format)
is the designated point (x-axis) value about which phase values are to be unwrapped. This point is called the . This would typically be a well-known point in a measurement such as the passband of a band pass filter.
This parameter is only available for the selection of .
For segmented traces, phase unwrapping is reset at the beginning of each segment.
See Also